Hi:
Im working in the MPC5643L_144pin ( LSM mode) . I'm using the Capture feature of the eTimer0 module to measure the external signal frequency. Input signal is connected to channel 4, channel 3 is Cascaded counter mode.
Test Result:
The test result is not correct .What's wrong with my project?
thanks
void etimer0_init(void)
{
ETIMER_0.ENBL.R = 0x0;//禁止通道
ETIMER_0.CHANNEL[3].CTRL1.R = 0x3804;
ETIMER_0.CHANNEL[3].COMP1.R = 0xFFFF;
ETIMER_0.CHANNEL[3].CCCTRL.R = 0x0265;
ETIMER_0.CHANNEL[3].CTRL3.R= 1;
SIU.PCR[99].B.IBE = 1; //etimer0_4
SIU.PSMI[7].B.PADSEL = 3;
ETIMER_0.CHANNEL[4].CTRL1.R = 0xF804; // cascaded mode, count up, rollover, count repeatedl
ETIMER_0.CHANNEL[4].COMP1.R = 0xFFFF;
ETIMER_0.CHANNEL[4].CCCTRL.R = 0x0265; // compare on COMP1 when counting up, COMP2 when counting down
// CAPT2 on falling edge, CAPT1 on rising edge, 2 entries
// free-running mode
ETIMER_0.CHANNEL[4].CTRL3.R = 1;
ETIMER_0.ENBL.R =ENBL3 | ENBL4;
}
main()
{
...........................
while{
while(!(0x0080 & ETIMER_0.CHANNEL[4].STS.R)){}; // wait for channel 1's capture2 flag
while(!(0x0080 & ETIMER_0.CHANNEL[3].STS.R)){};
capture_ch1[0] = ETIMER_0.CHANNEL[4].CAPT1.R;
capture_ch1[1] = ETIMER_0.CHANNEL[4].CAPT2.R;
capture_ch1[2] = ETIMER_0.CHANNEL[4].CAPT1.R;
capture_ch1[3] = ETIMER_0.CHANNEL[4].CAPT2.R;
capture_ch0[0] = ETIMER_0.CHANNEL[3].CAPT1.R;
capture_ch0[1] = ETIMER_0.CHANNEL[3].CAPT2.R;
capture_ch0[2] = ETIMER_0.CHANNEL[3].CAPT1.R;
capture_ch0[3] = ETIMER_0.CHANNEL[3].CAPT2.R;
capture_ch1[4] = ETIMER_0.CHANNEL[4].CAPT1.R;
capture_ch1[5] = ETIMER_0.CHANNEL[4].CAPT2.R;
capture_ch1[6] = ETIMER_0.CHANNEL[4].CAPT1.R;
capture_ch1[7] = ETIMER_0.CHANNEL[4].CAPT2.R;
capture_ch0[4] = ETIMER_0.CHANNEL[3].CAPT1.R;
capture_ch0[5] = ETIMER_0.CHANNEL[3].CAPT2.R;
capture_ch0[6] = ETIMER_0.CHANNEL[3].CAPT1.R;
capture_ch0[7] = ETIMER_0.CHANNEL[3].CAPT2.R;
SIU.GPDO[7].R ^= 0x1;
edge1 = capture_ch1[0]*65536 + capture_ch0[0]; // save 1st rising edge
edge2 = capture_ch1[1]*65536 + capture_ch0[1]; // save 1st falling edge
edge3 = capture_ch1[2]*65536 + capture_ch0[2]; // save 2nd rising edge
edge4 = capture_ch1[3]*65536 + capture_ch0[3]; // save 2nd falling edge
// calculate period, pulseH, pulseL, freq and duty
if(edge3>edge1)
{
counts = edge3 - edge1;
}
else
{
counts = (0xFFFFFFFF - edge1 +1) + edge3;
}
freq = (float)8000000.0/counts;
period = counts / (float)8000.0;
if(edge2>edge1)
{
counts = edge2 - edge1;
}
else
{
counts = (0xFFFFFFFF - edge1 +1) + edge2;
}
pulseH = counts / (float)8000.0;
pulseL = period-pulseH;
ETIMER_0.CHANNEL[3].STS.R = 0x00C0; // clear eTimer0 channel 3's capture1/2 flags
ETIMER_0.CHANNEL[4].STS.R = 0x00C0;
ETIMER_0.CHANNEL[3].CCCTRL.B.ARM = 1; // starts the input capture process
ETIMER_0.CHANNEL[4].CCCTRL.B.ARM = 1;
}
}
Hi,
This can easily happen, if the square signal is available on the pin and you debug/stop the code. In free-running capture mode the capture is still functional, and you configure the eTimer’s counter to be stopped in debug mode, thus if FIFO is empty, it can be filled with new values (same counter values as this is stopped).
So you can either:
- configure eTimer channels to run in debug mode too (CTRL3[DBGEN]) or better
- disable capture operation once you are going to read FIFO and calculate results, finaly enable capture again…use
while{
while(!(0x0080 & ETIMER_0.CHANNEL[4].STS.R)){}; // wait for channel 1's capture2 flag
while(!(0x0080 & ETIMER_0.CHANNEL[3].STS.R)){};
ETIMER_0.CHANNEL[3].CCCTRL.B.ARM = 0; // stop the input capture process
ETIMER_0.CHANNEL[4].CCCTRL.B.ARM = 0;
// read FIFO and calculate result, code can be stopped here
ETIMER_0.CHANNEL[3].STS.R = 0x00C0; // clear eTimer0 channel 3's capture1/2 flags
ETIMER_0.CHANNEL[4].STS.R = 0x00C0;
ETIMER_0.CHANNEL[3].CCCTRL.B.ARM = 1; // starts the input capture process
ETIMER_0.CHANNEL[4].CCCTRL.B.ARM = 1;
}
BR, Petr