#include "netifcfg.h" file not found error in MPC5748G: ENET_PING example.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

#include "netifcfg.h" file not found error in MPC5748G: ENET_PING example.

1,278件の閲覧回数
tejo2one
Contributor III

Hello,

 

I am working on NXP Gateway board which uses MPC5748G, I need to setup Ethernet communication and checking example codes. ENET_PING : found this example code but it doesnot build. Is there any example code using ethernet interface which works using MPC5748G.

Thank you in advance,

Tejo

tejo2one_0-1680545653829.png

 

0 件の賞賛
10 返答(返信)

1,251件の閲覧回数
tejo2one
Contributor III

Thanks for the response Lukas.

I apologize for mistake, I am using example "lwip_mpc5748g" not ENET_PING.

tejo2one_0-1680797030190.png

 

0 件の賞賛

1,245件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Exactly the same is working also for lwip example. Can you find the file in S32DS folder? Isn't the installation corrupted?

Regards,

Lukas

0 件の賞賛

1,239件の閲覧回数
tejo2one
Contributor III

I uninstalled and reinstalled S32DS., still same issue.

Can you share your code ?

0 件の賞賛

1,243件の閲覧回数
tejo2one
Contributor III
Lucas, I could not find this file.
For my reference what is the S32DS version you're using?
0 件の賞賛

1,191件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @tejo2one 

I used S32DS 2.1 and SDK 3.0.3.

I just found out that the file is not present in the S32DS installation folder but it's generated by processor expert, so I can see it in my project.

I will attach my project here, you can try to import it.

Regards,

Lukas

0 件の賞賛

955件の閲覧回数
tejo2one
Contributor III

Hello @lukaszadrapa ,

              Thanks for your code. I tried loading it in as a local project and when I give generate code command "netifcfg.c and netifcfg.h" are removed by tool.

               I felt my tool was corrupted so reinstalled S32DS again but same problem still exists.

Is there any link where I can download whole setup locally and install it? please support me its already taken lot of time.

 Thanks in advance.

Tejo

 

0 件の賞賛

943件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @tejo2one 

If you go to:

Help -> S32DS Extensions and Updates

and

Help -> About S32 Design Studio... -> Installation Details

... could you see if all these packages are installed? That's my setup which works:

lukaszadrapa_0-1683022143328.png

 

lukaszadrapa_1-1683022152941.png

There's no way to install this as a one single package.

Regards,

Lukas

0 件の賞賛

1,165件の閲覧回数
tejo2one
Contributor III

Hello Lukas,

 

Thanks for reply and code. I tried flashing your code but its stuck in HSM_Init during SSL_Init.

Is HSM firmware required to use TCPIP stack ?

 

Thanks & best regards,

Tejo

0 件の賞賛

1,158件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Please take a look at this thread:

https://community.nxp.com/t5/MPC5xxx/WolfSSL-on-MPC5748G-devkit/m-p/1460985

And also this one - it is possible to use SW implementation only:

https://community.nxp.com/t5/S32-SDK/using-wolfSSL-library-on-MPC5748G-board-with-out-HSM-firmware/m...

Regards,

Lukas

0 件の賞賛

1,256件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @tejo2one 

I can see no problem on my side. What I did:

File -> New -> S32DS Project from Example

Then I selected mentioned enet_ping example for MPC5748G.

Now the key point - it is necessary to generate the code by this:

lukaszadrapa_2-1680794091400.png

Or select in main menu: Project -> Generate Processor Expert Code.

Then you should be able to build the project.

Regards,

Lukas

 
0 件の賞賛