Hi!
I choose the Trigger source from ETIMER0_IN and the PWM_ODD ,but it can only to implement a Trigger.
Hi,
Input trigger signals are ORed.
As there is only 1 TGS you can only have 1 reaction on the input trigger.
I am not able to understand from your description what you are trying to achieve.
Peter
Peter
Hi,Thank's your answer.I'm trying to implement two input trigger signals that is not happen on the same time,and then i can get data of the
ADC channel when a corresponding input trigger was happened.
Hi,
If the signals are synchronous then it is possible to use CTU for 2 input triggers.
You just have to arrange 2 ADC command list to do so. ADC command list is double buffered and are updated on MSR.
it will looks like:
Peter