how to make a project running in ram

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to make a project running in ram

867件の閲覧回数
曾经怀念
Contributor II

Hi all,

       Who can provide a project that can run in RAM?

      What is the difference between the flash project and the ram project?

      (like LCF, memory copy  ???)

thanks

0 件の賞賛
返信
2 返答(返信)

752件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

Which microcontroller you use?

If you use MPC57xx or some MPC56xx which is supported by S32DS, I recommend you to download S32 Design Studio and look at the differences between linker files.

S32 Design Studio IDE|NXP 

If you use MPC56xx, you can download CodeWarrior. Create new project and check the differences between RAM and Flash target.

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 

If you have any other questions, please feel free to write me back.

Regards,

Martin

0 件の賞賛
返信

752件の閲覧回数
曾经怀念
Contributor II

thank you very much

I have another questions MPC5605B sdata issue

can you give me some tips?

0 件の賞賛
返信