how to configure processor expert for CAN ID filtering through pretended networking(MPC5748G)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to configure processor expert for CAN ID filtering through pretended networking(MPC5748G)

830 Views
FAISAL0323
Contributor II

Hi. I am trying to implement pretended networking for flexcan 0 by configuring processor expert as shown in figure but there is one problem,  when I select that flexcan 0 and give range for can ID filtering, processor expert is unable to generate code as it says that peripheral is already been used. how to fix that issue? since we already set configurations in PE(Processor Expert) ,so I want to add that pretended networking feature in already configured PE.

what I want to do is to set Mask for filtering  CAN IDs from 0x580 TO 0x5FF to keep ECU wake up. 

Please let me know if there is any solution. Thanks

processor i am using is MPC5748G

   

FAISAL0323_0-1634862807591.png

 

0 Kudos
Reply
1 Reply

803 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

one instance of FlexCAN peripheral module (or any other module) can be used by one component only. This error message can appear when you have two FlexCAN components and you try to assign the same "CAN_0" to both of them.

It looks like "cc_main_can" is also configured to use CAN_0.

Regards,

Lukas

 

0 Kudos
Reply