[elxr] (error #21) cannot find library -lmulti

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[elxr] (error #21) cannot find library -lmulti

ソリューションへジャンプ
1,762件の閲覧回数
tmduybk
Contributor II

Hi,

I download Example MPC5748G Flash RW GHS614.

But when I using command line "gbuild -top MPC5748G-Flash_RW-GHS614.gpj", cmd show Error:

[elxr] (error #21) cannot find library -lmulti

I attach image of an error. Thank you !

0 件の賞賛
返信
1 解決策
1,736件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

not sure what's the root cause here but the example is very simple piece of code, so you can only copy the code from main.c and add it to your project (to any IDE). No other files are needed or modified.

Regards,

Lukas

 

元の投稿で解決策を見る

1 返信
1,737件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

not sure what's the root cause here but the example is very simple piece of code, so you can only copy the code from main.c and add it to your project (to any IDE). No other files are needed or modified.

Regards,

Lukas