dmpc5777c seral boot loader and RAppID Boot Loader Utility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dmpc5777c seral boot loader and RAppID Boot Loader Utility

561件の閲覧回数
Alex5080
Contributor II

when I use RAppID Boot Loader Utility to dowload application. there is message is as attached picture.

on target board side,    use eSCI_A as boot serial . EVTO PIN is float. Bootcfg set as 01.

the error message told that  we should use CAN interface not serial(232) interface. In fact, we used uart (232) not CAN inteface.

Would you  please help to check it ? 

0 件の賞賛
2 返答(返信)

555件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Alex,

Just to better understand your setup: 

Have you downloaded .rbf file into your board first via JTAG?

RAppid BL does not support BAM "Hardware boot" for MPC57xx so BAM setup has no effect whatsoever.

Which board are you targetting - custom one of NXP EVB?

Stan

 

0 件の賞賛

543件の閲覧回数
Alex5080
Contributor II
1. don't download rbf file via JTAG. 2.target board is customer board. not NXP even board. 3. use eSCI_A as boot serial. 4. bootcfg configure as 01.
0 件の賞賛