adc_pal configuration for group convertion with EMIOS hardware trigger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

adc_pal configuration for group convertion with EMIOS hardware trigger

1,171件の閲覧回数
LyncLin
Contributor III

Hi,

I'm using ADC_PAL component of processor expert to configure for a EQADC conversion group triggered by EMIOS edge. When there are 4 adc channels in the group, the hardware trigger and conversion works fine. However, when I add another channel and there are 5 channels in the same group, it can't sample and conversion correctly.

Then I try to use software trigger to do the same test. It works fine with 4channels, but return STATUS_BUSY status with 5 channels. Enclosed with the project I'm using.

Is there any limitation in the number of conversions in one group?

タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,134件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, there no such limitation there, at least in case eQADC commands are being filled by DMA continuously. Are yo using streaming mode?

I am going to check your attachment as soon as possible.

0 件の賞賛
返信

1,124件の閲覧回数
LyncLin
Contributor III

Thanks for your reply. 

I check the RM of MPC5777C, the ADC fifo depth is four, is it root cause for this case?

What should I do if I want sample more than 4 channels in a single trigger, should I activate streaming mode?

0 件の賞賛
返信

1,094件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Certainly not, but you may use up to 8 command entries with streaming mode, in case configuration used does not continuously push command to the CFIFO (by DMA).

0 件の賞賛
返信