Waking up from LPU_STOP with pretended mode's TIMEOUT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Waking up from LPU_STOP with pretended mode's TIMEOUT

452 次查看
nimrodzarmi
Contributor II

Hey,

I've been struggling with getting in & out of LPU_STOP mode for quite some time.
I tried using the example everyone refers to.

It seems to get into LPU_STOP, where all cores are not running, but after waking it up with a random CAN fame on CAN_0, I think the MCU was stuck in LPU_RUN where only core 2 was running (I saw a small bump in current).

I'm not sure what I'm missing.

Is there a full example where the MCU wakes up back to full DRUN from timeout on CAN_0's pretended mode?
That example will not be board dependent at all, and should work on my board seemlesly.
I'll be able to work out the differences from there.

Thanks! 

标记 (1)
0 项奖励
回复
1 回复

389 次查看
nimrodzarmi
Contributor II

UPDATE:

Looks like I can get into LPU_STOP, but after sending a CAN frame that wakes up the MCU, it restarts.
At least the Z4 core does. I do not understand why, because I followed the published example.

0 项奖励
回复