Use multiple CAN buses (all 6) in mpc5606b

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Use multiple CAN buses (all 6) in mpc5606b

456 次查看
sundar19
Contributor III

Hi,

I use the startertrak dev kit mpc5606b. 

I just wanted to know how to use multiple CAN buses simultaneouly. 

for example ,

 

 

void CanTxMsg (uint32_t id, uint8_t mb, uint8_t dlc, uint8_t data[], uint8_t ext)
{
    uint8_t	i;

    if (ext)
    {
        CAN_1.BUF[mb].CS.B.IDE = 1; /* extended ID */
        CAN_1.BUF[mb].ID.R = id;    /* Tx ID extended */
    }
    else
    {
        CAN_1.BUF[mb].CS.B.IDE = 0; /* standard ID */
        CAN_1.BUF[mb].ID.B.STD_ID = (uint16_t)id; /* Tx ID standard */
    }
    CAN_1.BUF[mb].CS.B.RTR = 0;      /* no remote Tx request frame */
    CAN_1.BUF[mb].CS.B.LENGTH = dlc; /* # bytes to Tx */
    for (i = 0; i < dlc; i++) 
    {
        CAN_1.BUF[mb].DATA.B[i] = data[i]; /* Data to Tx */
    }
    CAN_1.BUF[mb].CS.B.SRR = 1;            /* Tx frame */
    CAN_1.BUF[mb].CS.B.CODE = CAN_TX_MSG;  /* Send msg */ 
}

 

 

 

The above is the function definition for using CAN 1 to transmit messages , should I replace "CAN_1" to "CAN_0" to use the 0th CAN bus?

To be precise:

1. initialize required CAN buses using RAPPID.

2. create my own function definition in CANdrv.c

for example, to use 0th CAN bus , I will replace all "CAN_1" with "CAN_0" and create a new function definition known as CanTxMsg0()

3. Declare the same as global funtion declaration in CANapi.h

For example , I will declare the above CanTxMsg0() as global function declaration

 

 

CanTxMsg0(uint32_t, uint8_t, uint8_t, uint8_t[], uint8_t) 

 

 

4.Call the function in main.c

For example, I will call the above function as 

 

 

CanTxMsg0 (2, 1, 8, (uint8_t *)msgOKCAN, 0);

 

 

 Is my procedure correct ? 

Thank you

标记 (2)
0 项奖励
0 回复数