Hi.
I am using the RDVCU5775EVM(based on mpc5775B) board and installed S32DS_Power_v2017.R1
RDVCU5775EVM board description says install SDK RTM 3.0.0 but I couldn't see it so I got SDK RTM 3.0.3
I followed the process and got the following error
Let me know the solution
The address below is the process referenced.
An error occurred after proceeding with '10. Import the SDK project to S32DS'.
Could we get help?
Thanks
Solved! Go to Solution.
The above issue has been resolved.
When I installed 'S32 Design Studio for Power Architecture® v2.1 - Windows/Linux', there was 'SDK RTM 3.0.0' inside and no error appeared in the post.
Thanks
The above issue has been resolved.
When I installed 'S32 Design Studio for Power Architecture® v2.1 - Windows/Linux', there was 'SDK RTM 3.0.0' inside and no error appeared in the post.
Thanks