Hi:
When I execute a for (unsigned short i = 0; i <5000; i ++) {} in the MPC5744P, It takes about 500us. When I execute a for (unsigned short i = 0; i <5000; i ++) { a = b+c;} in the MPC5744P, It takes about 1000us.The MPC5744P clock speed is 160MHz.But according to the MPC5744P reference manual, the '+' operator takes only one clock cycle, the '*' operator takes two clock cycles, Why this code takes so long time?Or what else should I use to speed up the execution?This question has bothered me for a long time and hope you can help me.
Thanks very much!
Hi, I have done in accordance with your method and found that for a n1 = n2 + n3 operation, the compiler requires seven instructions. The disassembly results are as follows:n1 = n2 + n3;
1 e_lhz r9, 10(r31)
2 e_rlwinm r10, r9, 0, 16, 31
3 e_lhz r9, 12(r31)
4 e_rlwinm r9, r9, 0, 16, 31
5 add r9, r10, r9
6 e_rlwinm r9, r9, 0, 16, 31
7 e_sth, 8(r31).
If I use the assembly instructions to achieve a "+" operation in MPC5744P, also need to use seven instructions to achieve this operation?
You may try to change optimization setting of you compiler to higher level.
Also you could try to define operand as register type like this
register int n1, n2, n3;
This definition places operand directly into register thus it could shrink generated code.
I have been in accordance with the second method you said to optimize the code and achieved some results.I carry out radar signal processing on MPC5744P.But the current program execution speed is still not meet the real-time requirements.I would like to know can i write assembly code in the MPC5744P ?If so, what is the instruction set for the MPC5744P and how can I use it in the MPC5744P?