The target may have entered reset escalation,please power cycle on the board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The target may have entered reset escalation,please power cycle on the board

1,114件の閲覧回数
ChenBowen
Contributor II

My MPC5744P can't connect with the S32DS,  it shows "The target may have entered reset escalation,please power cycle on the board'    How to solve this problem?

0 件の賞賛
4 返答(返信)

1,105件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could  you be more specific? What kind od debugger are you using? Was the device working before? Did you program anything to it?

Are the device working in stand-alone setup (no debugger). Are voltages in specified range according to datasheet?

Best regards,

Peter

0 件の賞賛

1,096件の閲覧回数
ChenBowen
Contributor II

I always use the OpenSDA debugger.  It works before.   Last time l did Flash erase and program on 5744P, l currently  need to finish a Bootloader Project.

0 件の賞賛

1,083件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,
The reset escalation from S32DS message is most probably false.

Your debugger is simply not able to connect to device because the device is in reset.

If you run the device after power on reset in stand alone (no debugger) mode and measure reset line via scope, do you see it permanently asserted? Are voltages in specified range. Especially 3.3V and 1.2V.

Best regards,

Peter

0 件の賞賛

1,001件の閲覧回数
ChenBowen
Contributor II

I don't have scope right now , so if it permanently asserted ,what to do?

0 件の賞賛