The question about the Force out logic for MPC5643L

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The question about the Force out logic for MPC5643L

503 次查看
edenli
Contributor V

Hi Guys,

(1)There are some question about the Force out Logic,the Figure 25-17.Force Out Logic in  MPC5643L Microcontroller
Reference Manual
  page672.shown as below:

pastedImage_2.png

1#:Abve Figure ,the Part A,there is a box that label D ,Force_Out and Q, the relationship between the three?

(2) in  MPC5643L Microcontroller Reference Manual  page708,shown as below:

pastedImage_12.png

2#:the content said the register(SWCOUT) is used to set the deadtime,i have some doubt to be confrimed,

2.1:How the deadtime is achieved ? I thought If We set the SWCOUT to 0,When the Q output the value 2,and the Mux output the OUT23-3=0,then the deadtime is achieved. 

for exzample:

frist,We set the SEL23_3 =10,then  OUT23_3 will insert the deadtime ;

second,IF we set  OUT23_3 =0,and the deadtime Zero will be insert,if we set OUT23_3 =1,the he deadtime one will be insert? is that right ?
2.2:is PWM23 is equal to PWMA,And PWM45 is equal to PWMB?

I don't know the PWM23_3 corresponds to which pin of the hardware?

Thank you !

0 项奖励
0 回复数