According to the UM,This bit can be written only in Freeze mode。But I'm already in freeze mode,It's no use writing 1,The register value was found to be 0 when debugging with lauterbach,Before that,FRZ bir is 1, FRZACK bit is 1, and HALT bit is 0。Even if I don't set HALT to 0,When I've set up the MAXMB bit, HALT automatically goes to 0。
Could you tell me the reason why I failed to write IRMQ?