The Error about debug the dual motor project for MPC5643L

cancel
Showing results for 
Search instead for 
Did you mean: 

The Error about debug the dual motor project for MPC5643L

388 Views
edenli
Contributor V

Hi Guys,

I download the dual motor control project from NXP :http://www.nxp.com/downloads/en/apps/MTRCKTDPS5643L_SW.exe ,and i import the project into S32 V1.1,i compile it there is no errror,but when i debug it into the board ,there some error shown as below:

189771_189771.pngpastedImage_2.png

and the code don't download into the MPC5643L.

How to solve it ?

the Attachment is the Project

Original Attachment has been moved to: Test_9.zip

0 Kudos
1 Reply

296 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I have loaded your code into micro flash with Lauterbach debugger without any issues.

However code reports FCCU errors and after execution micro goes into safe state.

So you should check your debugger settings and loading script as your issue is there.

Peter

0 Kudos