TGN2-0054-30-36 Motor Data sheet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TGN2-0054-30-36 Motor Data sheet

Jump to solution
3,341 Views
alimeraj
Contributor IV

Hi, 

Can someone please help me with the TGN2-0054-30-36 motor data sheet. This motor is used in  MCSPTR2A5775E development kit. I have 2 of these kit however I cant find the motor data sheet anywhere. I need the motor parameters to design my control system. 

Thanks,

Ali

0 Kudos
Reply
1 Solution
3,299 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

See please attachment, that's what I got from them.

Hope it helps.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
8 Replies
3,337 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
3,334 Views
alimeraj
Contributor IV

Hi Lukas,

Thanks for sending the links.

I have one more motor that came with NXP kit which is bit different to TGN2-0054-30-36 and I cant seems to find the motor parameter for TGT2-0032-30-24 in the links you sent me. could you please point me where I can find the motor parameters for this motor.

 

Thanks,

Ali

0 Kudos
Reply
3,318 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Ali,

I can't find details on their site too. I have only these numbers for the motor:

0.32Nm, 30V, 5.2A, 3000rpm

If it is not sufficient, please send them an email and request more details: info@tgdrives.cz

Thanks,

Lukas

0 Kudos
Reply
3,313 Views
alimeraj
Contributor IV

Thanks for looking Lukas, 

I need inductance, resistance and BEMF value for my control. I don't have RLC meter otherwise I would have measure it. I tried to contact tgdrive but they never contacted back. I was thinking if you guys have any direct contact with them since your kits have their motors?

Thanks,

Ali

0 Kudos
Reply
3,308 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hmm, I do not have direct contact but let me try to ask them. Maybe I will have more luck.

Regards,

Lukas

0 Kudos
Reply
3,306 Views
alimeraj
Contributor IV

Thanks Lukas, really appreciated.

0 Kudos
Reply
3,300 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

See please attachment, that's what I got from them.

Hope it helps.

Regards,

Lukas

0 Kudos
Reply
3,296 Views
alimeraj
Contributor IV

Hi Lukas,

This is great, this is exactly what I was looking for.

Thank you very much.

Kind Regards,

Ali

0 Kudos
Reply