Something about flash memory for MPC5675K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Something about flash memory for MPC5675K

436 Views
1329306846
Contributor III

Hello everyone,

   For some reasons, I need to use CAN bootloader to download program for MPC5675K. But there are some questions puzzled me .

   First, I know that we can read-while-write between different banks, but whether it means that we can not read-while-write in the same bank. I really hpe to get the answer.

Someone tell me yes , but I had dowmload bootloader program in the memory start in 0x100000 and then download application program in the memory start in 0x4010.Finally, the application program run well. I do not know whether it can make bad effect in the future.

Second, in the Mid Address Space an high Address Space , the first (lower addresses) 16 bytes (128 bits) of every 32-byte aligned range are stored in CFM0 and the last 16 bytes(128 bits) are stored in CFM1.

I really do not know why and it had puzzled me for a long time . Really hope someone can help me.

Best regards.

Guang Yao

]A%A)XSPO7W[[F2{MD`U5QV.png

0 Kudos
0 Replies