Hello,
I would like to control the solenoid valve using the MPC5644A. According to NXP, the MPC5644A is suitable for transmission control. I did not see such a thing in the MPC5644A datasheet and manuel reference.
I want to using the dither method. Which module can be used to control the solenoid valve.
Could you give us an example.
Hi,
Thank you very much for replies.
Yes, that is i want to do.
I can not see because my friends are wrongly suggesting. :smileyhappy:
Thx.
Hi, apparently you mean Reaction Module.