Thanks for the help!
I have another question. When disassembling the code I get assembler code like this:
00000034: E2EF se_bne *-34 ; 0x00000012
The ";0x00000012 at the end of the line confuses me. If reading the document "MCU_Power-Architecture_compiler.pdf" it says
"
Anything following a ; character is considered to be a comment, except in GNU
compatibility mode, where ; is a statement separator.
"
Becauase this line gives the compilation error ">end of line expected" it's is probably another statement. If this "statement" is removed there are no problems when compiling but it would probably not work since some code has been removed.
Is the disassembler doing something wrong? How should the statement look like instead of " ; 0x00000012"
Hi,
I wrote simple example for you. Use the following function:
asm void function()
{
/*SIU.MCR[18] = 0x0200
* load value to r0, load register address to r5, store value to register
**/
e_li r0,0x0200
e_lis r5,0xc3f9
e_or2i r5,0x0064
e_sth r0,0(r5)
/*SIU.GPDO[18] = 0x1*/
se_li r0,1
e_lis r5,0xc3f9
e_or2i r5,0x0612
e_stb r0,0(r5)
}
Call this function in your main function. You can check correct register settings using debugger.
Btw, semicolon means comment in assembly language.
Regards,
Martin
Hi again!
Thanks!! This works fine in the debugger when singel-stepping the line:
e_sth r0,0(r5)
but if a break-Point is set at the next line:
se_li r0,1
and then singel-stepping from this line the output is not set. It seems like the OBE bit is not set in the last case.
Is there a smart way to make sure that the OBE bit is set?
I better mention that if this should work at all for me I have to start with setting ME_RUN_PC0 DRUN = 1 and ME_PCTL68 RUN_CFG = 0. All this modifications are done in MPC5604B_Startup.c
Hi,
at first, check Peripheral Status Register 2 in mode entry module. SIU module has to be enabled, otherwise it is not possible to write to the module.
Also you can look at the following function.
void InitModesAndClks(void) {
ME.MER.R = 0x0000001D; /* Enable DRUN, RUN0, SAFE, RESET modes */
CGM.FMPLL_CR.R = 0x02300100; /* 8MHz xtal: Set PLL0 to 48 MHz */
ME.RUNPC[0].R = 0x000000FE;/* enable peripherals run in all modes */
ME.RUN[0].R = 0x001F0074; /* RUN0 cfg: IRCON,OSC0ON,PLL0ON,syclk=PLL */
/*Mode Transition to enter RUN0 mode:*/
ME.MCTL.R = 0x40005AF0; /* Enter RUN0 Mode & Key */
ME.MCTL.R = 0x4000A50F; /* Enter RUN0 Mode & Inverted Key */
while (ME.GS.B.S_MTRANS) {} ; /* Wait for mode transition to complete */
while(ME.GS.B.S_CURRENTMODE != 4) {};/* Verify RUN0 is the current mode */
}
Could you please tell me, which debugger you use? I tested in Lauterbach, but it works correct. Also in this case, breakpoints should not affect code execution. Could you please also provide me some screens of your problem? I am not able to reproduce it.
Regards,
Martin
Hi Martin!
Sorry, I should have provided you with this information from the beginning. I'm using Code Warrior for MCU version 10.6.
Some explanation of my problem. I have to set an input to another unit also containing a uC (This unit is from another Company). I have to set it very fast since it must be done before the uC on the other unit is awake. The first try was to set it as early as possible in main after the run-mode settings but this turned out to not be fast enough. Then I tried to do it as soon as possible after boot and this is where I'm struggling now. I made the assumption that Everything written between boot and main() has to be written in assembler since this is how it looks like in the platform code. Is this assumption right??
Here some screens from the debugger:
First I'm singel-stepping the line where OBE is set and there you can see in Registers that this bit has been set.
second try I set the break-Point at the next line and now OBE is not set.
The entire code in MPC5604B_Startup.c now looks like this:
asm void __startup(register int argc, register char **argv, register char **envp)
{
nofralloc /* explicitly no stack */
/* frame allocation */
// Enable SIUL in DRUN mode
//ME.RUNPC[0].B.DRUN = setBit;
se_li r0,1
e_lis r9,0xc3fe
e_lwz r8,-16256(r9)
e_insrwi r8,r0,1,28 ; e_rlwimi r8,r0,3,28,28
e_stw r8,-16256(r9)
//ME.PCTL[68].B.RUN_CFG = 0;
se_li r0,0
e_lis r9,0xc3fe
e_lbz r8,-16124(r9)
e_insrwi r8,r0,3,29 ; e_rlwimi r8,r0,0,29,31
e_stb r8,-16124(r9)
/*SIU.MCR[18] = 0x0200
* load value to r0, load register address to r5, store value to register
**/
e_li r0,0x0200
e_lis r5,0xc3f9
e_or2i r5,0x0064
e_sth r0,0(r5)
/*SIU.GPDO[18] = 0x1*/
se_li r0,1
e_lis r5,0xc3f9
e_or2i r5,0x0612
e_stb r0,0(r5)
// call standard application initialization
bl __start
}
Regards Bengt
Hi Bengt,
I tested your code and you are correct about the behavior. It seems, there is some synchronization problem. So the only idea which I have is to do mode transition after you set RUNPC and PCTL. So add the following code under the RUNPC and PCTL settings:
e_lis r9,0x3000
e_add16i r9,r9,0x5AF0
e_lis r8,0xC3FE
e_stw r9,-0x3FFC(r8)
e_lis r9,0x3001
e_add16i r9,r9,-0x5AF1
e_lis r8,0xC3FE
e_stw r9,-0x3FFC(r8)
This code is equivalent to:
ME.MCTL.R = 0x30005AF0; /* Enter DRUN Mode & Key */
ME.MCTL.R = 0x3000A50F; /* Enter DRUN Mode & Inverted Key */
Try this solution and eventually write me back if it is usable for you.
Regards,
Martin