STN2100 responds with? (invalid command) when giving STFPA, ATCRA command

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

STN2100 responds with? (invalid command) when giving STFPA, ATCRA command

816 次查看
priya_p
Contributor IV

I am using MPC5748G microcontroller and it is programmed to communicate with external OBD transceiver STN2100 via UART terminal. In the datasheet of STN2100, it does mention it support STFPA, ATCRA commands but whenever I am sending STFPA command as STFPA 7E8, 008 \r\n  its responding back with "?" , means invalid command. Why it is happening, when it is specified in the datasheet clearly that it support this command. 

RESPONSE OF STN2100

priya_p_0-1645513687742.pngrefer

 

REFERENCE and PROGRAMMING  MANUAL for stn2100

priya_p_1-1645513718364.png

 

标记 (1)
0 项奖励
2 回复数

808 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

STN2100 is not our product, this is a question rather for manufacturer of this device.

Regards,

Lukas

0 项奖励

804 次查看
priya_p
Contributor IV

Yes, I am well aware about it. I posted it in here in hope that If anyone is there who have worked with OBD, could help me to clarify my doubt.

0 项奖励