SPT some of the problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPT some of the problems

836 Views
yinlei
Contributor III
  • I am learning SPT related instructions, about LOOP and NEXT. I want to make the rangeFFT loop 64 times between these two instructions, while changing the input and output addresses in the SRAM, but does not solve the problem

void fft_spt_fft256(uint32_t input_start, uint32_t output_start, tdPar* par){
    uint32_t wr_val;
    uint32_t i;

    // Define how to read words from RAM
    if( par->chipset == chipsetKestrel ){
      // 7 word SKIP in SRAM, 1 word continuous(Used to read a channel in 8-channel Tile 4)
      wr_val = 0x01007001;
    }
    else{
      // 2 word SKIP in SRAM, 1 word continuous(Used to read a channel in 3-channel Tile 4)
      wr_val = 0x01002001;
    }

    /* Mem location of the first input & location where first output is placed
       are populated by dummy values (0xDEADBEEF)
       They are modified after array initialization */
    uint32_t instructSet[] = {

       // LOOP - 64 times   新增修改
       0x14000040, 0x00000000, 0x00000000, 0x00000000,

       // Load Samples
       // Sign extend, direct, 16-bit real pack
       // synchronous, VEC_LEN = 64(0x040) * 64-bit SRAM words = 512 bytes
       // The 512 bytes contain all 256 * 2 byte SDADC samples for 1 chirp
       // PDMA SRAM(SAMPLE_SRAM_START) -> OPRAM (0x8000)
       // x word SKIP in SRAM, y word continuous(Used to read a channel in n-channel Tile 4)
       0xA18D0040, input_start, 0x80000000, wr_val,


        // ADD command: increment SRAM offset in FFT result buffer to next chirp
        // ADD, immediate data, no left shift, 24bit modulo?
        // SRC1 is work register 0, DEST is work register 0
        // SRC2 is work register 0(n/a)
        // immediate data = 0x000010000000: WR[0].IM += 0x1000, WR[0].RE += 0x0000
          0x0C00001F, 0x00000000, 0x00000000, 0x00001000,

      // FFT 265 RDX4 instruction w/ real input
      // input @0x8000, twiddles @0x4000, window @0x4500 output @0xA000
      // pad with 4 LSBs
      //0x84000100, 0x80008100, 0x00000101, 0x7fff0040,
      // Win and pre-scaling << 8
      0x84000100, 0x80008100, 0x45000101, 0x00010250,
        

      // fixed scaling
      // RDX4, round 0 and pre-scaling << 1
      0x88030100, 0x81009000, 0x40000101, 0x00000010,
      // RDX4, round 1
      0x8a110100, 0x9000A000, 0x40000101, 0x00000000,
      // RDX4, round 2
      0x8a210100, 0xA0009000, 0x40000101, 0x00000000,
      // RDX4, round 3
      0x8a310100, 0x9000A000, 0x40000101, 0x00000000,
    
      // PDMA transfer of output to SRAM
      // Sign extension, direct address, 24-bit complex
      // PDMA OPRAM (0x9000) -> SRAM (OUTPUT_SRAM_START), synchronous,
      // Vec len = 256 units, no skip (continuous transfer)
      0xA1870100, output_start, 0x00080000, 0x01000004,
      
      // ADD command: increment work register for next loop
      // ADD, immediate data, no left shift, 24bit modulo?
      // SRC1 is work register 1, DEST is work register 1
      // SRC2 is work register 0(n/a)
      // immediate data = 0x000008000080: WR[1].IM += 0x0008(move to next bin), WR[1].RE += 0x0400
      0x0C00001F, 0x00080008, 0x00000000, 0x00000400,

      // NEXT loop
      0x18000000, 0x00000000, 0x00000000, 0x00000000,

      // Stop Cmd
      0x10000000, 0x00000000, 0x00000000, 0x00000000      
};
      
    //Write the set of commands into memory for SPT to fetch
    for(i=0;i<sizeof(instructSet)/sizeof(uint32_t); i++)
    {
      wr_val = instructSet[i];
      *(vuint32_t*)((FFT_INSTRUCTION_START) + (i*4))= wr_val;
    }
    
    SPT.CS_STATUS0.R = 0xFFFFFFFF;       // RESET all status register
     
    //SPT.GBL_CTRL.R = 0x0;               // RESET Ctrl
    //SPT.GBL_CTRL.B.SPT_EN = 0;           // RESET SPT
    
    SPT.CS_PG_ST_ADDR.R =FFT_INSTRUCTION_START;     // instructions start address
    
    //SPT.GBL_CTRL.R = 0x1F;             // Enable SPT, ACQ & start command sequencer
    
    SPT.GBL_CTRL.R = 0x1D;           // Enable SPT & Program start control
    //SPT.GBL_CTRL.B.SPT_EN = 1;           // Enable SPT & Program start control
    
   while ((SPT.CS_STATUS0.R&0x8)!=0x8){} // Wait until SPT finished commands

}

 The program will stop at the last statement

  “ while ((SPT.CS_STATUS0.R&0x8)!=0x8){} // Wait until SPT finished commands”

Labels (1)
Tags (1)
0 Kudos
2 Replies

509 Views
taokang
Contributor III

Hi,

if it is command errors,you can read the relevant bit of SPT_CS_STATUS1 , SPT_DMA_ERR_STATUS
, SPT_HW_ACC_ERR_STATUS  ,if it is non-command errors,you can read the relevant bit of SPT_MEM_ERR_STATUS
, SPT_DMA_ERR_STATUS, SPT_HW_ACC_ERR_STATUS , All bits of SPT_HIST_OVF_STATUS0 , All bits of SPT_HIST_OVF_STATUS1 .Last,before the start,best to let  the command sequencer at RST state.


0 Kudos

509 Views
yinlei
Contributor III

Thanks for your help, I found the wrong flag in the registerBut I still did not solve the problemAs I mentioned earlier, I just want to change the input and output address in a loop, I do not know where the problem

0 Kudos