SPC5741P and SPC5744P Controller Pinout is same?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPC5741P and SPC5744P Controller Pinout is same?

879 Views
muthukrishnanp
Contributor II

Hi,

Please confirm the 32BIT Controller Pinout is pin to pin same SPC5741P and SPC5744P?

Regards

Muthukrishnan P

0 Kudos
Reply
3 Replies

656 Views
muthukrishnanp
Contributor II

Hi Martin,

 

Thank you for support.

We have face issue RESET Pin is Pulled low always @10K Pull up Resistor.

Pull up resistor we modified 4k7 and 3k3 values still it is pull low.there after 100E resistor used for pull up

now RESET Pin Voltage is 0.7V. What is the actual current need RESET Pin during Power on restet and debugging mode.  Data sheet defined 15mA. 3.3V and 100E pull up resistor is sufficient still voltage drop persist. 

any recommendation is need for RESET Pin.

0 Kudos
Reply

656 Views
muthukrishnanp
Contributor II

Hi Martin,

Thank you for support.

We have face issue RESET Pin is Pulled low always @10K Pull up Resistor.

Pull up resistor we modified 4k7 and 3k3 values still it is pull low.there after 100E resistor used for pull up

now RESET Pin Voltage is 0.7V. What is the actual current need RESET Pin during Power on restet and debugging mode.  Data sheet defined 15mA. 3.3V and 100E pull up resistor is sufficient still voltage drop persist. 

any recommendation is need for RESET Pin.

0 Kudos
Reply

656 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

yes, there is the same pinout for MPC5744P and MPC5741P.

Regards,

Martin

0 Kudos
Reply