SENT(Single Edge Nibble Transmission) with MPC5746R

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SENT(Single Edge Nibble Transmission) with MPC5746R

ソリューションへジャンプ
1,346件の閲覧回数
fanshichencao
Contributor I

Where can I find the SENT example of MPC5746R,I refer to the user manual for SRX register configuration, but it is not work successful.

Thank!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,200件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

within S32 Design Studio you can find SDK example called "srx_fast_dma_mpc5746r".

The purpose of this example is to highlight the usage of the SRX Peripheral Abstraction Layer implemented over the SENT module on MPC5746R CPU using the S32 SDK API. The application will read values from a TLE4988 SENT Hall effect sensor.

Also you can refer to AN4856 (https://www.nxp.com/docs/en/application-note/AN4856.pdf ) it isi for MPC5744P but teh SENT module is similar.

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,201件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

within S32 Design Studio you can find SDK example called "srx_fast_dma_mpc5746r".

The purpose of this example is to highlight the usage of the SRX Peripheral Abstraction Layer implemented over the SENT module on MPC5746R CPU using the S32 SDK API. The application will read values from a TLE4988 SENT Hall effect sensor.

Also you can refer to AN4856 (https://www.nxp.com/docs/en/application-note/AN4856.pdf ) it isi for MPC5744P but teh SENT module is similar.

BR, Petr

0 件の賞賛
返信
1,200件の閲覧回数
fanshichencao
Contributor I

1.I found the AN4856.But the hardware vector mode INTC used in this example.And I use soft vector mode INTC.

2.I downloaded and installed the S32 SDK, but I didn't find example called "srx_fast_dma_mpc5746r". What should I do to see the demo?How to use SDK in S32 studio?

Thank you very much!

0 件の賞賛
返信
1,200件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

within S32DS create new Project from example ...

pastedImage_1.png

pastedImage_2.png

BR, Petr

0 件の賞賛
返信
1,200件の閲覧回数
fanshichencao
Contributor I

Hello Petr,

Got it.Thank you very much!

0 件の賞賛
返信