S32R274 reset_B keeps low

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R274 reset_B keeps low

818 Views
wangzhebuaa
Contributor I

Hi all,

       I am debugging my board based on S32R274 now, but I can encountered a problem: my PE micro USB mulitlink can not connect my device. 

       After checking the JTAG interface signals, I found that the the signal on S32R274 RESET_B pin always keep in LOW after I power on the system(either with or without the JTAG interface connected). And actually, the pin is pull-up to V3.3 by a 4.7K resistor.

       An in S32R274 reference manual Table4-1, it is described that the RESET_B is kept in LOW during POR and RESET stages. It means that my S32R274 is kept in POR/RESET stage, and there is some problem with my S32R274?pastedImage_2.png

pastedImage_1.png

      Is there anybody can tell me how can I get throught the problem? Thanks 

Tags (2)
0 Kudos
Reply
2 Replies

675 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, the reset_b is kept low during reset phase. (reset signal is negated)

User cannot easily recognize which reset phase the device actually is and it is not important.

If the device works correctly it will leave reset after phase 3 with any issues.

The question is what you were doing with micro?

What do you see on reset line after power on reset (POR)? Do you see signal toggles before it stays in permanent reset or do you see direct permanent reset after POR.

regards,

Peter

0 Kudos
Reply

675 Views
wangzhebuaa
Contributor I

How can I know which reset stage it stay in?

0 Kudos
Reply