Hello,
I develop an application whose need to interface an rotary sensor that generate these signals bellow:
These signals are used to determinate the RPM and the direction of rotation of wheel. So on MPC5121e I want to use one pair of GPT timer: GPT2 and GPT3, respectively on PSC10_4 and PSC11_4 pins.
for the first test I generate the two signals with simple push button and deglitching circuit connected on PSC10_4 and PSC11_4.
From reference manual I write a code that to do :
Define IOCONTROL_BASE = IMMRBAR + 0xA000
Define GPT_BASE = IMMRBAR + 0x0B00
CONFIGURE I/O
Write 0x0000_0183 into STD_PSC10_4 @(IOCONTROL_BASE + 0x2E4)
Write 0x0000_0183 into STD_PSC11_4 @(IOCONTROL_BASE + 0x2F8)
Set timer mode
Write 0x000D_0400 into GPT2_MODE @(GPT_BASE + 0x20)
Write 0x000C_0400 into GPT3_MODE @(GPT_BASE + 0x30)
Set COUNTER
Write 0x0001_0000 into GPT2_COUNTER @(GPT_BASE + 0x24)
Write 0x0001_0000 into GPT3_COUNTER @(GPT_BASE + 0x34)
Set PWM
Write 0x0000_0000 into GPT2_PWM @(GPT_BASE + x028)
Write 0x0000_0000 into GPT3_PWM @(GPT_BASE + x038)
Clear STATUS
Write 0x0000_001F into GPT2_STATUS @(GPT_BASE + 0x2C)
Write 0x0000_001F into GPT3_STATUS @(GPT_BASE + 0x3C)
Enable timers
Write 0x000D_1401 into GPT2_MODE @(GPT_BASE + 0x20)
Write 0x000C_1401 into GPT3_MODE (GPT_BASE + 0x20)
At this point my program is in pause, and I generate 1~10 pulses on ODO_1 with ODO_2 at 0.
And when with my program I want to read CAPTURE into GPT2_STATUS (CAPTURE = (@(GPT_BASE+0x2C) >> 16) &0xFFFF), I have CAPTURE randomly equal to 0~65535 instead of to have CAPTURE equal to 1~10.
David
解決済! 解決策の投稿を見る。
What method is used for timer pulse generation?
Is there bounce of your signals?
Usually bounce produces similar behavior.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
What method is used for timer pulse generation?
Is there bounce of your signals?
Usually bounce produces similar behavior.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pavel Chubakov,
We have resolved this problem with a low-frequency square signal generator in low impedance. And at this time, the number of events on GPT2-GPT3 is right in regards to number of events on inputs of MPC5121e.
Thank you for your assistance.
Best regards
David