Resolver and PWM in MBDT without eTPU - MPC5775E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Resolver and PWM in MBDT without eTPU - MPC5775E

174 Views
TLin3
Contributor III

Hello NXP Community,

I would like to develop motor control application software for a MCSPTR2A5775E motor DevKit with MPC5775E board using the MBDT.

Two essential functions, resolver feedback, and three-phase PWM output signals, are using the eTPU. The MBDT does not have feature blocks/functions set up for the eTPU-related functions.

Here is the same topic, but did not get the support to have those two functions achieved successfully.


https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MPC5775E-Generate-PWM-and-Evaluate-Reso...

 

I have also opened a topic to seek for support:


https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Evaluate-Resolver-and-Generate-PWM-in-M...

 

Would you please kidly support this topic, please?

 

Thank you

0 Kudos
Reply
0 Replies