Require MPC5775E MSC config demo code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Require MPC5775E MSC config demo code

460 Views
haiping_guo
Contributor I

Hi,

I are using MPC5575E. Could you help to provide MPC5575E's DSPI usage in the TSB Configuration demo code for reference? Thanks!

 

Best Regards,

Haiping 

0 Kudos
1 Reply

396 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

In the past I have tested DSPI serialization what’s already configuration similar to microsecond bus (on this device the feature is called timed serial bus TSB):

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5746R-DSPI-serialization-S32DS-Power-...

Microsecond bus protocol consist additional features to the SPI. These would be needed to configure and add to mentioned example and you will get MSC example:

1 ) serialization of internal timers

2) LVDS terminal pairs (positive and negative) for data output and clock

3) changes in data format

For SOUT and SCLK it is needed to choose and configure pins properly according excel sheet embedded to the device’s RM.

0 Kudos