RAppID Boot Loader for Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RAppID Boot Loader for Linux

ソリューションへジャンプ
4,260件の閲覧回数
yibbidy
Contributor V

Hi,

I may need to update the firmware in a MPC5643L remotely.  LINFlex_0's UART is connected to an embedded linux board.  Does a linux command line version of the RAppID boot loader exist?  I suspect that I might have to write one myself based on the description of the Boot Assist Module in the reference manual and maybe snooping the serial port of the Windows CLI version.  Some source code of the existing versions would come in handy, is any obtainable?

Thanks, Shaun

タグ(1)
0 件の賞賛
返信
1 解決策
4,016件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello,

As far as i know there is no Linux version of RAppid Bootloader. The PC-side application is written in C# and currently it support just Windows platform.

Unfortunately we do not provide a source code.

It's based on CCP protocol (https://automotivetechis.files.wordpress.com/2012/06/ccp211.pdf)

See more details about Rappid Bootloader here: Overview of RAppID Bootloader|NXP 

Hope it helps.

Stan

元の投稿で解決策を見る

4 返答(返信)
4,017件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello,

As far as i know there is no Linux version of RAppid Bootloader. The PC-side application is written in C# and currently it support just Windows platform.

Unfortunately we do not provide a source code.

It's based on CCP protocol (https://automotivetechis.files.wordpress.com/2012/06/ccp211.pdf)

See more details about Rappid Bootloader here: Overview of RAppID Bootloader|NXP 

Hope it helps.

Stan

3,960件の閲覧回数
Wally0258
Contributor I

Hi Stanish,

Due to CAN bus hardware limitation, I'd like to write a small software to support CAN bootloader via PCAN. Could you please provide CCP CRO and DTO ID? thanks.

0 件の賞賛
返信
4,015件の閲覧回数
yibbidy
Contributor V

Hi Stanislav,

I didn't think I'd have much joy on the source code or linux front.  Thanks very much for your links, especially to the CCP protocol, that is very useful - I am not in the automotive sector and I did not know it existed.

Regards, Shaun

0 件の賞賛
返信
4,015件の閲覧回数
jfrey
Contributor IV

Shaun James wrote:

Hi Stanislav,

 

I didn't think I'd have much joy on the source code or linux front.  Thanks very much for your links, especially to the CCP protocol, that is very useful - I am not in the automotive sector and I did not know it existed.

 

Regards, Shaun


You may get lucky looking at the pyccp module: GitHub - pySART/pyccp: ASAM CAN Calibration Protocol for Python https://github.com/pySART/pyccp/blob/master/setup.py

0 件の賞賛
返信