Question about SBC MC33908 Failsafe release mechanism

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about SBC MC33908 Failsafe release mechanism

748 Views
littledino2112
Contributor I

Hi all,

I'm integrating this SBC IC into an ECU system. Currently i'm having some confusions on the mechanism to release the Failsafe line (FS0b) after start-up, or wakeup from LPOFF mode. From my understanding, after waking up, the FS line is asserted (LOW) and the Reset Error Counter is 1. To release the FS line, i need to service the WD 7 consecutive times (assuming the WD refresh counter is kept at default value - 6). My system currently has a defined task used to service the WD at 100ms period (WD windows is configured at 128ms). Using this approach though, i will need 700ms after waking up to release the FS, which is way too long and unacceptable in my system.I'm thinking of 2 possible solutions:

- Change the WD refresh counter to 1. With this setting, it'll take 2 good WD refresh to release the FS line, which takes 200ms. This number is still way too slow and i would prefer a much shorter time to release the FS line.

- Change the WD windows to 3ms, service the WD using timer interrupt, then after the FS line is released, i'll need to change the WD windows back to 128ms so the OS task can be used to pet the dog. This would satisfy the requirement but seems overly complicated to me and may cause synchronization issue in the system as well.

My question is should there be a better solution to this? What is the regular mechanism that is being used to release the FS line?

 

Regards,

Labels (1)
Tags (2)
0 Kudos
1 Reply

471 Views
aero72
Contributor III

Dear Hoang,

My advice would be to set the WD window to be a short period, get the counter to be zero as quick as you can and then set the codeword for FS0 release.

During the initialisation task of our application, I deliberately set a PIT interrupt at 1ms, get the WD counter to zero with a 3ms window, then release FS0_b.

Yes it's annoying, but I'm afraid these days functional safety requires everyone to be more diligent in the code they write.

You're then able to set the WD window at a time to suit your fault tolerant time interval, and call your watchdog kick code at a time to match.

Regards