Problems about use the ICU of MCAL of MPC5744P

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems about use the ICU of MCAL of MPC5744P

628件の閲覧回数
qm1013
Contributor III

hello, I have some problems about the ICU configuration of the MCAL of MPC5744P. 

Bellow is the configuration of the ICU, but when the PWM signal in on the input pin , the programs can not go to the ISR of the ICU. Could you give me a demo of the ICU configuration for capture the PWM signal?

The MCAL Version is :4.0.3

pastedImage_1.png

Regards, 

meng

タグ(4)
0 件の賞賛
1 返信

552件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Hello,

From what I know, the MCAL package MPC574XP_MCAL4_0_RTM_2_0_2 have already had an example for capturing the PWM signal with ICU. Please find it in "MPC574XP_MCAL4_0_RTM_2_0_2\MPC574XP_MCAL4_0_RTM_2_0_2_Sample_Application"

Best regards,

Hung.

0 件の賞賛