Pop up dialog with "The target may have entered reset escalation..." when flashing by S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pop up dialog with "The target may have entered reset escalation..." when flashing by S32DS

3,871 Views
yuhaopan
Contributor II

I'm working with DEVKIT-MPC5748G board, and control target via JTAG Pemicro Multilink Universal .

I flash the target ,During that progress I accidently hit the reset button.

After then I can not flash any more.

It pops up dialog with "The target may have entered reset escalation, Please power cycle the board" when flashing by S32DS.

The attached file is the snap shoot .

I want to know how to recover it?

Thanks!

Yuhao Pan

7 Replies

2,594 Views
mailnakul
Contributor I

Hi, In mean time, is there any solution for this problem ? Any updates or its still impossible to recover the device ? Can NXP refund for this failure ? 

0 Kudos

2,594 Views
yuhaopan
Contributor II

Does it happen in MPC5xxx?

No way to recover?

Thanks!

Yuhao Pan

0 Kudos

2,594 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

this problem is related to MPC5748G, MPC5746C and it's derivatives only.

We have already discus this thing with application and design team and unfortunately, there is no way, how to recover the device. 

Regards,

Martin

2,594 Views
vamsikavety
Contributor I

Hello @Martin

I got exact same error. I build .elf file, compiled using GHS compiler in custom eclipse based build environment. And then I am flashing .elf file on MPC5746C via JTAG Pemicro Multilink Universal using s32ds IDE.  I have received pop up  "The target may have entered reset escalation, Please power cycle the board" when flashing with S32DS.

Does anyone found solution ? Do you think my chip was bricked ? 

I have already updated PEmicro plugin in s32ds, but i am not able to fix it. What should I do to recover my device?

0 Kudos

2,594 Views
laxmanraoravada
Contributor I

I am also faceing same issue.If any one haveing solution please update. I bought new one and suddenly it's failed.

0 Kudos

2,594 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

I have bad news for you. With almost 100% probability, your microcontroller is dead. Please check threads below.

MPC5748G can not attach JTAG 

https://community.nxp.com/message/890274 

If you have any other questions, please feel free to write me back.

Regards,

Martin

2,594 Views
yuhaopan
Contributor II

我和美国工程师沟通了

https://community.nxp.com/thread/455563

下面是回复

pan yuhao

于 2017-07-13 15:04, b55689 回复:

RE: POP UP DIALOG WITH "THE TARGET MAY HAVE ENTERED RESET

ESCALATION..." WHEN FLASHING BY S32DS

reply from Martin Kovar in MPC5xxx - View the full discussion

0 Kudos