Part number:-  MPC5668G. Using mqx rtos 4.0.2 and code worrior 10.2. Most of cards are working fine but in some card when we run application it stuck in ivor trap or in other places and application can’t run furthermore. The number of such faulty card is

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Part number:-  MPC5668G. Using mqx rtos 4.0.2 and code worrior 10.2. Most of cards are working fine but in some card when we run application it stuck in ivor trap or in other places and application can’t run furthermore. The number of such faulty card is

482件の閲覧回数
anandkhandelwal
Contributor I

Part number:-  MPC5668G.

Using mqx rtos 4.0.2 and code worrior 10.2.

Most of cards are working fine but in some card when we run application it stuck in ivor trap or in other places and application can’t run furthermore.

The number of such faulty card is reached 100.

Same application is running on other cards without any change.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)