Need help for MPC5668G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help for MPC5668G

Jump to solution
4,881 Views
ravikiranbhairu
Contributor II

Hello,

 

Does anyone have hands-on experience with MPC5668G dual-core EVB?

I am starting a new Project and have this EVB delivered recently.

 

1. Do i need to make any changes in Default Jumper Settings to start using the board, say for running simple toggle_led code?

2. We are using Codewarrior IDE v2.8 for MPC56xx along with PE Mico for flashing and Debugging. Am i missing something?

 

Any sort of help is highly appreciated.

 

Regards

Ravikiran

Labels (1)
1 Solution
4,691 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the LEDs (DS4 - DS7) are not connected to GPIOs on MCU. You need to connect PH10 pin (pin 10 on connector P28) to any pin on connector P15...

Lukas

View solution in original post

0 Kudos
Reply
9 Replies
4,691 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it is not necessary to change default jumper settings. You can use attached project for initial tests. It was written in CodeWarrior 2.7 and tested with PEmicro. It will work also in CW 2.8.

Regards,

Lukas

4,691 Views
ravikiranbhairu
Contributor II

Hello Lukas,

Thank you for the example project. Do you have a project for blinking/toggling user LED's?

Regards,

Ravikiran

0 Kudos
Reply
4,691 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Attached.

4,691 Views
ravikiranbhairu
Contributor II

Hello Lukas,

Thanks again. But when i flash the attached code onto the board, i dont see LED toggling. Do i need to make any changes in Jumper connections? or connect the LED port to some pin? 

Regards

Ravikiran

0 Kudos
Reply
4,692 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the LEDs (DS4 - DS7) are not connected to GPIOs on MCU. You need to connect PH10 pin (pin 10 on connector P28) to any pin on connector P15...

Lukas

0 Kudos
Reply
4,691 Views
ravikiranbhairu
Contributor II

Hello Lukas,

Do you have any other code examples for this board?

Regards,

Ravikiran

0 Kudos
Reply
4,691 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

attached you will find a couple of examples I found in my repository...

Regards,

Lukas

4,691 Views
ravikiranbhairu
Contributor II

Thank you Lukas. It worked. I had by mistake connected PH5 to P15 which was giving me LED high all the time.

Regards,

Ravikiran

0 Kudos
Reply