My BAM(MPC5534) doesn't work well!!!!!!!! Please Help me.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

My BAM(MPC5534) doesn't work well!!!!!!!! Please Help me.

968 次查看
wanglong
Contributor II

I would like to implement the BAM MPC5534A

 

I use a CW for MPC55xx and MPC56xx 2.9 and a MPC5534.

I have created a project using the Project Wizard feature of the Code warrior.

According to the advice of Lukas, I have edited the lcf file for __ start () function is moved to the starting address of SRAM (0x40000000).

Then I have found the problem.

Program entry address offset oxoooo0030

S705400000301A

If I have edited the lcf file for __ start () function is moved to the starting address of SRAM (0x40007000).

S705400070301A

How can I solve this problem?Lukas Zadrapa

2/5000
标签 (1)
0 项奖励
6 回复数

743 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

And one more thing - be aware there are three errata related to BAM:

http://www.nxp.com/assets/documents/data/en/errata/MPC5534revA.pdf 

0 项奖励

743 次查看
wanglong
Contributor II

thank you very much for your help

0 项奖励

743 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

attached you will find project which I modified to start at 0x4000_0000. I can see in the map file that the start function begins at this address. 

Regards,

Lukas

743 次查看
wanglong
Contributor II

Why is my application not running, and I'm going to set it up in the bam mode in your way

0 项奖励

743 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

lukaszadrapa‌ is on vacation today. He will write you back later in this week.

Regards,

Martin

0 项奖励

743 次查看
wanglong
Contributor II

Thank you very much

0 项奖励