MPU_1 MPC5777C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPU_1 MPC5777C

495件の閲覧回数
Othmane1
Contributor II

Hi,

I'm trying to use the MPU_1 on core1 (not using MPU_0), and when i do the configuration for the region descriptors, the moment i enable the MPU_1 i go to the exception(IVOR1) and when i check the registers of the MPU_1 during debug the MPU is not even enabled, in fact the moment i got through the code instruction that enable the MPU all everything resets!!!!

0 件の賞賛
返信
1 返信

467件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

MPU0 can only protect PRAMC_0 (means address range 0x40000000–0x4003FFFF)
MPU1 can only protect PRAMC_1 (means address range 0x40040000–0x4007FFFF)

That's probably the point.

0 件の賞賛
返信