I want to konw MPC5744 FlexCAN module hasn't a send completion entry interrupt function and a receive completion entry interrupt function?
I through computer software to send a standard data frame to my evaluate board , I through check interrupt flag to read data. But i want to process the receive data by receiving interrupts, I set FlexCAN Interrupt mask regiseter to enable interrupt receive function. But this code is not triggle interrupt function,the corresponding interrupt register is already in set 1.
解決済! 解決策の投稿を見る。
Hi,
CAN[nbModule]->IMASK1.R = 0x00F00000; does not enable MB8 and MB9 interrupt. In fact it enables MB23-MB20 interrupts.
You should use CAN[nbModule]->IMASK1.R = 0x00000300; //set MB[8] receive interrupt and MB[9] send interrupt
BR, Petr
5744中的can通信,你处理过接收端可以让接收端一对多通信吗?
5744中CAN通信,接收多个不同messgeID的模式(接收端一对多通信),你能成功吗?我没搞定
Hi,
CAN[nbModule]->IMASK1.R = 0x00F00000; does not enable MB8 and MB9 interrupt. In fact it enables MB23-MB20 interrupts.
You should use CAN[nbModule]->IMASK1.R = 0x00000300; //set MB[8] receive interrupt and MB[9] send interrupt
BR, Petr
FlexCAN interrupt setting is follow
INTC_0.PSR[524].B.PRIN = INT_CAN_PRIORITY; //CAN ISR IRQ CPU degree
CAN[nbModule]->IMASK2.R = 0x00000000; //FlexCAN module
CAN[nbModule]->IMASK1.R = 0x00F00000; //set MB[8] receive interrupt and MB[9] send interrupt
Is there anything wrong with my setup?
Make certain you're clearing the interrupt and also 'New data in buffer' flags by writing a '1' to the relevant register bit to clear it. Only by doing this will you know whether you're getting a new message or re-processing an old one.
Hi,
I'm sure that the corresponding flag bits in the interrupt flag register are clear, and I'm sure that the data received by querying is up to date, not the previous one.
The code received a standard data frame by compute software ,the relevant interrupt mask register bit is enable ,and relevant interrupt flag register is set.
The program does not perform interrupt subroutines .
thanks