Hi all,
I use MPC5777C on Green Hills - Multi, i build demo code to blink led base on Example MPC5748G PIT ISR .
Now if demo code run PIT no interrupts it ok but I user PIT with interrupt it hang. I think it do not find address of vector table when PIT interrupt occurs.
I set MPC5777C_IsrVecTab.c file,
set PIT interrupts is location at 301 in vector table,
void INTC_Init(void) { //-1-------------------------------------------------------------------- /* The Block Configuration Register is used to configure options of the INTC. Initialize INTC for software vector mode */ INTC.MCR.R = 0x00000000; //-2-------------------------------------------------------------------- /* configure IVORx offsets This file also includes a trap for all core exceptions, excluding IVOR4 exceptions which have seperate handler */ e200zX_Interrupt_Setup(); //-3-------------------------------------------------------------------- /* configure Interrupt Base pointer Set INTC ISR vector table base address */ INTC.IACKR.B.VTBA = (uint32_t) &IntcIsrVectorTable[0]; //-4-------------------------------------------------------------------- // assign VECTOR TABLE address // INTC_0.IACKR[0].R = (uint32_t) IntcIsrVectorTable; //-5-------------------------------------------------------------------- // set lowest priority to enable interrupts from higher ones INTC.CPR.B.PRI = 0; //-6-------------------------------------------------------------------- // assing required peripheral priorities //INTC.PSR[226].R = 0x8001; // PIT0 INTC.PSR[301].B.PRC_SEL = 0x00; // PIT0 INTC.PSR[301].B.PRI = 0x01; // PIT0 //-7-------------------------------------------------------------------- // Enable interrupts asm(" wrteei 1"); }//INTC_Init
set
.equ INTC_IACKR, 0xFFF48010 # Interrupt Acknowledge Register address
.equ INTC_EOIR, 0xFFF48018 # End Of Interrupt Register address
Where am I missing ?
Do you have complete example of this PIT with interrupt ? Can you give me references ?
Thanks & Regards
D.Hung
Original Attachment has been moved to: MPC5777C_IsrVecTab.c.zip
Thank you ! Code it run ok. I see you changes Function to Setup the Core Interrupt Registers. Do you have document explaining the changes ?
#=================================================
# Function to Setup the Core Interrupt Registers
#=================================================
e200zX_Interrupt_Setup:
#IVPR = address base used with IVOR's
e_lis r5, __IVPR@h
e_or2i r5, __IVPR@l
mtIVPR r5
se_bmaski r3,0
se_and r3,r5
e_add16i r5,r3,0x00@l
mtivor0 r5
e_add16i r5,r3,0x10@l
mtivor1 r5
e_add16i r5,r3,0x20@l
mtivor2 r5
e_add16i r5,r3,0x30@l
mtivor3 r5
e_add16i r5,r3,0x40@l
mtivor4 r5
e_add16i r5,r3,0x50@l
mtivor5 r5
e_add16i r5,r3,0x60@l
mtivor6 r5
e_add16i r5,r3,0x70@l
mtivor7 r5
e_add16i r5,r3,0x80@l
mtivor8 r5
e_add16i r5,r3,0x90@l
mtivor9 r5
e_add16i r5,r3,0xA0@l
mtivor10 r5
e_add16i r5,r3,0xB0@l
mtivor11 r5
e_add16i r5,r3,0xC0@l
mtivor12 r5
e_add16i r5,r3, 0xD0@l
mtivor13 r5
e_add16i r5,r3,0xE0@l
mtivor14 r5
e_add16i r5,r3,0xF0@l
mtivor15 r5
se_blr
.size e200zX_Interrupt_Setup,$-e200zX_Interrupt_Setup