[MPC5777C] How can i cause exception error or unidentified interrupt?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MPC5777C] How can i cause exception error or unidentified interrupt?

1,363 Views
jongminna
Contributor III

Hi, Dear

Our development environment here

MCU : MPC5777C

OS : ETAS RTA OS

Compiler : Windriver diab 5.9.4

 

I want to exception handler test, so I have to make some kind of exception error.

Refer to e200z760RM(315page), MPC5777C has Machine check(IVOR1) and Program(IVOR6).

I don't know that what i have to do for causing a exception error.

 

In specific, I want to test "Illegal instruction exception", "Data cache parity error" and Exception handler which is cased by specified error.

In other words, I want to fault injection method above them.

 

Please let me know what i have to do.

 

Thank you.

Labels (1)
0 Kudos
3 Replies

880 Views
gvictorio
Contributor III

Hello Jongmin,

Have you tried the instruction se_illegal? that seems to be exactly what you need for the illegal instruction exception.se_illegal.PNG

Other ideas may be:

  • Try to write to a register of a peripheral that is not enabled.
  • Try to write to an reserved/invalid memory address

For the parity error, I'm not sure if trying to read from a RAM location that has not been initialized (never written) would do the trick.

0 Kudos

880 Views
jongminna
Contributor III

Thank you for your answer.

I have solved this question.

First of all, For the illigal insturction error, I try to execute instruction at the unused area.. Then exception error is arised.

Cache parity error is arised by cache controller, cache error injection.

Is it right solution?

0 Kudos

880 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

when you access memory (either instruction fetch or data load/store) and bus error occurs (unimplemented memory, ECC error...) then IVOR1 is triggered regardless of MSR[ME].

pastedImage_0.png

Read the chapter "7.6.2 Machine Check Interrupt (IVOR1)" in core reference manual for more details:

http://www.nxp.com/files/32bit/doc/ref_manual/e200z760RM.pdf

If a bus error does not occur during instruction fetch but invalid opcode is loaded (or se_illegal is used) then IVOR6 is triggered.

Yes, it is possible to inject the error to cache:

pastedImage_4.png

Cache errors will trigger IVOR1 exception. See the tables:

Table 7-10. Error Report Machine Check Exceptions

Table 7-11. Asynchronous Machine Check Exceptions

... in core reference manual.

Regards,

Lukas

0 Kudos