MPC574XP can't switch tasks when there is floating-point operation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC574XP can't switch tasks when there is floating-point operation

942 次查看
darcyxu
Contributor II


If there is floating-point operation in the project, the RTOS cannot switch tasks normally. If the floating-point operation is turned off before and after the open interrupt, it can be normal.
When using floating point arithmetic, which registers are required to be pushed into the stack when the task is switched?
It is best to provide a project with FREERTOS with floating point operations.

0 项奖励
回复
0 回复数