MPC574XG CPU is locked

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC574XG CPU is locked

1,075 Views
sijiahao
Contributor III

Hi

I have a problem with MPC574XG(Calypso),  the CPU is locked! “debug port fail” due to censorship.

The debugger is Trace32 from Lauterbach, this is the error informantion:

152794_152794.jpg1.jpg

according to the debugger_mpc5500.pdf on Trace32, we think the CPU might be locked.

152810_152810.jpg2.jpg

 

We also tried to enter the keycode to unlock it, but failed.152811_152811.jpg3.jpg

 

Can you help me to fix this? or any suggestions?

 

Best Regards

Sijia

Labels (1)
5 Replies

777 Views
petervlna
NXP TechSupport
NXP TechSupport

Did you play with UTEST memory area where censorship is stored?

0 Kudos

778 Views
sijiahao
Contributor III

I think yes. the board was downloaded with a wrong elf by someone else, which may edit this UTEST part.

0 Kudos

778 Views
petervlna
NXP TechSupport
NXP TechSupport

If this is the case, then there is way to recover from this state.

You have to replace microcontroller.

778 Views
jlim
Contributor II

I am having a similar problem after incorrectly modifying part of the UTEST region. Although, mine does not show any additional information other than "debug port fail". Can I still recover the device?

0 Kudos

778 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I would try to decrease debugger frequency to 1MHz

pastedImage_0.png

Although I don't know the reason it helps to me as I have the same problem with certain devices.

0 Kudos