[MPC5748G] Shared RAM implementation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MPC5748G] Shared RAM implementation

2,838 Views
yulianmatev
Contributor III

Hello all,
I have two projects a "Bootloader" and an "Application".
and I would like to configure a RAM segment (128 bytes, 0x4000100--0x400017F) which is accessible
by both of them, and they can exchange data through it.

 

My setup:

  • Hw: Custom board
  • MCU: MPC5748G 1N81M
  • Debugger: Laurterbach Trace32
  • Compiler: GHS Multi 6.1.6

This is what I did in order to implement it:
1. Configure a "shared_ram" RAM section inside Bootloader .ld file. 

2. Configure a "shared_ram" RAM section inside Application .ld file.
3. I modified startup asm code which initializes complete RAM (__ghs_ramstart -- __ghs_ramend) with 0xe800e800
so shared ram is skipped. (Note from the asm comment: This code initializes the ECC bits of the targets's SRAM by filling it with branch-to-self opcode) 

4. "shared_ram" is configured as non cache-able inside SMPU

Everything works fine when I am using the debugger,"Bootloader" and an "Application"are able to exchange data through this shared data.
The problem occurs when I run the target without debugger.
Using debug pins I am able to detect that software "crashes" the first time when a read access to the shared ram
(the one which is not initialized on purpose) is performed. Writing to this RAM is possible without an issue.

In the above sentence  "crashes" mean that software is not taking its expected path and no interrupt service routine is entered.

No special configurations for MEMU and FCCU are performed. 

Any ideas are welcome, thank you in advance!

Tags (2)
0 Kudos
Reply
3 Replies

2,464 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I suppose that between bootloader and application you are performing reset, is it so? If yes which kind of reset (functional/destructive)?

0 Kudos
Reply

2,464 Views
yulianmatev
Contributor III

Yes, switching between bootloader and application is performed with 'functional' reset

0 Kudos
Reply

2,464 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Have you checked shared ram content in application entry point (that is before SRAM initiazliation)? Do you see ECC errors there (mostly shown as '????') ?

0 Kudos
Reply