MPC5748G Ethernet Port in PHY Mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G Ethernet Port in PHY Mode?

1,810 Views
mmundt
Contributor I

Hi all,

is it possible to configure one of the MPC's ethernet-ports to "PHY" mode? We want to connect a MAC device via the Mii interface to the Calypso... Unfortunately I can only find information of how to run the Calypso in MAC Mode, in the manual.

 

Thank you in advance

Michael

Labels (1)
0 Kudos
Reply
2 Replies

1,106 Views
AROK
Contributor I

Main difference between MAC and PHY MII mode is the clock generation? The Calypso should be able to generate the RX and TX clock.

0 Kudos
Reply

1,106 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

What do you mean by “PHY” mode?

The MPC5748G includes just MAC device (ENET module) which can be connected with external PHY via MII interface.

External Ethernet controllers (MAC or MAC+PHY) are usually connected with the MCU over parallel external memory interface, which is not available on the MPC5748G.

BR, Petr

0 Kudos
Reply