MPC5746C FCCU NCF[0] Flash Reset Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746C FCCU NCF[0] Flash Reset Error

479 Views
shijie_zheng
Contributor III

The description of NCF[0] in the manual is“Flash reset error:
Sideband signal from flash to indicate that flash encountered faults during its reset reads.
This is caused by ECC double bit detection as well as the coherency checks done on the test
row reads”

Based on this description, I can't determine if this error only occurs on CPU reset? or, it can be generated when accessing flash,because ECC errors can occur at any time flash is accessed.

Can anyone help explain this description?

Thank you .

0 Kudos
2 Replies

426 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Based on this description, I can't determine if this error only occurs on CPU reset?

Yes, this error is triggered when there is a fault during flash initialization/test in reset phase 2.

pastedImage_24.png

or it can be generated when accessing flash,because ECC errors can occur at any time flash is accessed.

ECC errors during the device operation out of reset are reported in NCF[22] NCF[23].

regards,

Peter

0 Kudos

426 Views
shijie_zheng
Contributor III

Dear Peter,Thank you for your help,your explanation is very helpful。

0 Kudos