MPC5744P flexcan Application for receiving 63'ID question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P flexcan Application for receiving 63'ID question

498 Views
toddchou
Contributor I

Dear Sir 

Good day! I had a issue that was flexcan rx on MPC5744P devkit . On this case , I ued can0 on board and want to receive 63' can id . I set it in S32DSPA IDE as below : 

status_t CAN_Init(void)
{

uint8_t i ;

uint8_t j ;

uint8_t PS=1;

flexcan_data_info_t dataInfo =
{
.data_length = 8U ,
.msg_id_type = FLEXCAN_MSG_ID_EXT
};

flexcan_id_table_t full_id_table [ i * j ];

        for ( i = 1 ; i < 10 ; i++ )

            {

                  for ( j = 1 ; j<8 ; l++) 

                        {

                            if ( i < 2 ) {

                                 full_id_table [ i * j ] ={ (uint32_t ) ( 0x18000000 | (uint32_t)((j+1)<<16) | (uin32_t)                                                                          (PS<<8) | (uint32_t)(i)} ;

                                 } else 

                                     {

                                          full_id_table [ ((i-1) * j)+7 ] ={ (uint32_t ) ( 0x18000000 | (uint32_t)((j+1)<<16)                                                                                         | (uin32_t)(PS<<8) | (uint32_t)(i)} ;

                                      }

 

                        }

            }

FLEXCAN_DRV_Init(INST_CANCOM1, &canCom1_State, &canCom1_InitConfig0);

FLEXCAN_DRV_SetRxMbGlobalMask(INST_CANCOM1,FLEXCAN_MSG_ID_EXT,0x18FFFFFF);

FLEXCAN_DRV_ConfigRxFifo(INST_CANCOM1,FLEXCAN_RX_FIFO_ID_FORMAT_A,&full_id_table);

uint8_t temp ; 

for ( temp = 1 ; temp <63 ; tempe++ )

{

FLEXCAN_DRV_ConfigRxMb(INST_CANCOM1,temp,&dataInfo,full_id_table[temp])

}

}

Then I run the receiving function , I find the each mailbox always was in STATUS_CAN_BUFF_OUT_OF_RANGE . 

How can i slove this issue or may you provide me the more canId free receive in one mailbox sample code by the S32D

 

 

 

 

 

0 Kudos
2 Replies

476 Views
toddchou
Contributor I

Hello Sir 

Thank you 

0 Kudos

481 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if enabling RXFIFO some MBs are occupied by Rx FIFO and ID Filter table. This is determined by CTRL2[RFFN] setting. In flexcan component "RxFIFO ID filters number" parameter specifies this

PetrS_0-1621326286806.png

 

So for example for 64 filter elements (RFFN=7), MB0-21 are used by RXFIFO and ID table.

Thus if you want to configure additional regular MBs for receiving/transmitting, MBs 22-63 can be used. You cannot config MB1, MB2 and so on as you have.

BR, Petr