MPC5744P SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P SPI

2,278 Views
donnerx
Contributor II

I try to program for MPC5744 SPI, now I can get the SCK but I can't test any signal from the SOUT pin .

wenn I write to PUSHR, I see the TXFR get the correct data, but it doesn't send it, even all the 5 TXFR is filled.  Please help me. thank you!

hier is my code:

#include "derivative.h" /* include peripheral declarations */

unsigned int data;
void sys_config(void)
{
MC_ME.RUN_PC[0].B.DRUN=1;//open all pheriphral clock in DRUN mode
MC_ME.DRUN_MC.B.SYSCLK=2;//use pll0 to SYSCLK

//config PLL0 200Mhz
MC_ME.DRUN_MC.B.XOSCON=1;//Open XOSC in DRUN mode
MC_CGM.AC3_SC.B.SELCTL=1;//select XOSC as source of pll0;
PLLDIG.PLL0DV.R = 0x50000000 |0x00020000 |0x00002000 |0x0014 ; //predefined PLL0 divider register
MC_ME.DRUN_MC.B.PLL0ON=1;//Enable pll0;

/*
//config ADC_CLK
MC_CGM.AC0_SC.B.SELCTL=2;//Select pll0 as ADC_clk source
MC_CGM.AC0_DC2.R=0x80010000;// ADC_CLK=PLL0/(1+1)
*/

//config DSPI_CLK
MC_CGM.SC_DC0.R=0x80030000;//set PBRIDGEx_CLK 50mhz

//enter DRUN
MC_ME.MCTL.R = 0x30005AF0;
MC_ME.MCTL.R = 0x3000A50F;

//wait until done
while(!MC_ME.GS.B.S_PLL0); //ME_GS Wait for PLL stabilization.
while(MC_ME.GS.B.S_MTRANS);//Waiting for end of transaction
while(MC_ME.GS.B.S_CURRENT_MODE != 0x3);// ME_GS Check DRUN mode has successfully been entered
}

void SPI0_padconfig()
{
//config DSPI0
//config CS0
SIUL2.MSCR[36].B.SSS = 1; //Config C[4] as CS0
SIUL2.MSCR[36].B.OBE = 1; //Enable output buffer
SIUL2.MSCR[36].B.SRC = 3; // Full strength slew rate

SIUL2.MSCR[37].B.SSS = 1; //C[5] as SCK
SIUL2.MSCR[37].B.OBE = 1; //Enable output buffer
SIUL2.MSCR[37].B.SRC = 3; // Full strength slew rate

SIUL2.MSCR[38].B.SSS = 2; //C[6] as SOUT
SIUL2.MSCR[38].B.OBE = 1; //Enable output buffer
SIUL2.MSCR[38].B.SRC = 3; // Full strength slew rate

SIUL2.MSCR[39].B.IBE = 1; //Enable input buffer of C[7]
SIUL2.IMCR[41].B.SSS = 1; //C[7] as input pin SIN
}

void init_SPI0()
{
SPI_0.MCR.R = 0x80000001; //master mode, halt
SPI_0.MODE.CTAR[0].R = 0x78021004; //config baud rate
//DBR=0,FMSZ=1111,CPOL=0,CPHA=0,LSBFE=0,PCSSCK=00,PASC=00,PDT=00,PBR=10
//CSSCK=0001,ASC=0000,DT=0000,BR=0100
SPI_0.MCR.B.HALT = 0x0; //start spi0
}

void read_data_SPI_0(void)
{
while (SPI_0.SR.B.RFDF != 1){} //Wait for Receive FIFO Drain Flag = 1
data =SPI_0.POPR.R; //Read received data
SPI_0.SR.R = 0xDA0A0000; // Clear ALL status flags by writing 1 to them
}

int main(void)
{
int cont;
sys_config();
SPI0_padconfig();
init_SPI0();
/* Loop forever */
while(1)
{
SPI_0.PUSHR.PUSHR.R = 0x08015678; // Transmit data
cont=SPI_0.SR.B.TXCTR;
while(SPI_0.SR.B.TCF!=1); //Wait for transfer complete
read_data_SPI_0();
}
}

Labels (1)
Tags (1)
0 Kudos
3 Replies

1,288 Views
金广陈
Contributor II

能把你的SPI 程序发给我一个吗 谢谢啦

0 Kudos

1,288 Views
donnerx
Contributor II

I find the reason.. I write the code SIUL2.MSCR[38].B.SSS = 2; //C[6] as SOUT, it should be SIUL2.MSCR[38].B.SSS = 1; //C[6] as SOUT. 

Then , C[6] is used as SOUT.

0 Kudos

1,287 Views
金广陈
Contributor II

Hi

Could you please send me one of your SPI? Thank you

If the library function version is better

0 Kudos