MPC5744P NCF[13] fault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P NCF[13] fault

584件の閲覧回数
Xjianjian
Contributor I

I recently encountered an issue with FCCU not being able to enter configuration mode.it was found that the NCF[13] fault was triggered when the watchdog reset.and NCF[13] faults can not be cleared.

 

0 件の賞賛
3 返答(返信)

570件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, if this fault happens in debug mode (i.e. with attached debugger) then it is OK as this fault may be set when an external debug tool is connected and has to be ignored while the tool is connected.  

This statement is valid for NCF faults 11, 12, 13, 33, 34, 35, 36, 37, 38, 39, 44, 45, 69

 

If it happen without debugger we may investigate it further.

0 件の賞賛

556件の閲覧回数
Xjianjian
Contributor I

Thank you for your reply! No debugger was connected when the problem occurred.For the same software program, some hardware samples behave abnormally, while most of them behave normally  

Is there any investigation direction you can provide?

タグ(1)
0 件の賞賛

527件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Also there is an erratum. I guess it could be the issue.

davidtosenovjan_0-1621926403716.png

How you read the fault? If you stop code execution at breakpoint, you are in debug mode. To eliminate debug mode completely, it is needed to send message over some serial bus ideally (UART terminal, CAN and so).

0 件の賞賛