MPC5744P FCCU fault (NCF[56,57,58]) cannot be injected issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P FCCU fault (NCF[56,57,58]) cannot be injected issue

498 Views
Zhongling_Lang
NXP Employee
NXP Employee

Hi,

1.Now my customer test fault injection in FCCU module on mpc5744p and the NCF[56/57/58] cannot be injected, but in RM said that this three NCFs can be set and cleared.

2.This issue actually exist when I tested on MPC5744p devkit board(use the SDK code<fccu_fault_injection_mpc5744p> and sample code in our community). So why the RM information is inconsistent with our test results.

3.On the other hand, we test the fault injection on other MCU(mpc5746r,mpc5775e) and also have mismatch with RM information. may be some other information we should pay attention.

pastedImage_3.png

pastedImage_4.png

0 Kudos
2 Replies

407 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

You are right.

There is documentation ticket in place for quite some time. So the fix should be in near future.

Remove the fake fault injection capability for the NCF[56], NCF[57] and NCF[58] from the table 7-33. FCCU Non-Critical Faults Mapping in the chapter 7.12.3.1 Fault inputs.

regards,
Peter

0 Kudos

407 Views
Zhongling_Lang
NXP Employee
NXP Employee

Hi Peter,

Thanks for you reply, I will also update some fault injection mismatch with RM on MPC5746R and MPC57775E. 

0 Kudos