MPC56xx DSPI: PIN 213

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC56xx DSPI: PIN 213

614件の閲覧回数
robertwynn
Contributor I

Hello,

I am using Codewarrior 11.1 and have a SPC5634MMLU80 XRJ2001 1M35Y (176pin) processor.

I have been using DSPI_B (DSPI_B_SOUT on GPIO[104]) and the configuration works fine.

I have a new board with DSPI_B_SOUT on GPIO[213] I can not get it to work. GPIO[213] seems to mirror the SCK signal not the SOUT signal.


SIU .PCR[213].B.PA = 2; // does not work (this has been checked on two boards)

SIU .PCR[104].B.PA = 1; // does work

Is there something that I have to change because [213] has WKPCFG and NMI functionallity?


Thanks

 

0 件の賞賛
3 返答(返信)

591件の閲覧回数
robertwynn
Contributor I

Thanks David. I will rewire the board.

0 件の賞賛

601件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I have seen this in the past and I was answering:

"I can confirm observed behavior. I have found that SIU_IREER[NMIRE] SIU_IREER[SWTRE] act the same way and blocks PCR setting."

 

0 件の賞賛

598件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I checked previous communication and this has been reported and doc ticket probably has been raised. But as it is currently old device, no new RM has been issued.

One yet note that EVB board has jumper J9 choosing external pull-up or pull-down what can influence it as well.

davidtosenovjan_0-1618925965543.png

0 件の賞賛