MPC5676R GPIO Behavior / Datasheet unclear

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5676R GPIO Behavior / Datasheet unclear

2,301件の閲覧回数
joachimhofmann
Contributor I

SPC5676R  - Version Clarification / Behavior of Flexray GPIO Pins at Reset

 

Dear Team,

I would like to get clarification with regards to the Advance Datasheet MPC5676R Rev. 4, 16 Feb 2016

 

On page 85ff the Flexray/GPIOs are described with respect to their during and after RESET behavior.

 

A text denotes two options "for REV1 Devices" and for all other devices.

See Attachment

 

Currently Revision "K3" is current with a corresponding Maskset and Errata Document 3N23A.

 

It is totally unclear what "Revision 1" is supposed to be and what behavior these Pins on K3 devices really have.

 

Please clarify.

 

With regards

Joachim Hofmann

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,221件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

The only qualified revision is Rev 1.3 (with mask 3N23A)

Mentioned note is related to Rev 1.0. On your device it is -/Up.